Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10.0.3 - Maintenance Pack 8 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Dear Siemens PLM NX Customer,

Maintenance Pack 8 for NX 10.0.3 is now available on the Siemens PLM Download Server.

NX 10.0.3 MP8 is an accumulation of fixes built for installation on top of Windows 64-Bit and Linux 64-Bit images of NX 10.0.3.

To select the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Full Product Download page, Enter “10.0.3.mp08” (including the quotes) in the Search box to see a list of links to the release letter and available release packages.

Alternatively, the release packages can be found in the file navigator by selecting the ‘NX’ button and then navigating through the directory structure by selecting "Product updates > Maintenance-packs > Nx10 >
platform]".

Sincerely,

Ben Broad

Siemens PLM Software

3 REPLIES

Re: NX 10.0.3 - Maintenance Pack 8 Announcement

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

When I click on the download link, I get this message:

 

GTAC_insecure.PNG

Re: NX 10.0.3 - Maintenance Pack 8 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom
Thanks @cowski1, I'll look into it.

Ben

Re: NX 10.0.3 - Maintenance Pack 8 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

The GTAC Tools team has assured me that it is safe to continue if you receive this message. They are making a change and this error will no longer be present in approximately one week.

You can either click the "Advanced" to continue, or use Internet Explorer to download the file.

Ben