Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10.0.3 - Maintenance Pack19 Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Dear Siemens PLM NX Customer,

Maintenance Pack 19 for NX 10.0.3 is now available on the Siemens PLM Download Server.

NX 10.0.3 MP19 is an accumulation of fixes built for installation on top of Windows 64-Bit and Linux 64-Bit images of NX 10.0.3.

To select the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Full Product Download page, Enter “10.0.3.mp19” (including the quotes) in the Search box to see a list of links to the release letter and available release packages.

Alternatively, the release packages can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: Product updates > Maintenance-packs > Nx10 > [platform].

Sincerely,

Ben Broad

Siemens PLM Software