Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 Basic Curves

Legend
Legend

I seemed to have misplaced my "dialog bar" for basic curves.

any suggestions as to getting it back?

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
7 REPLIES 7

Re: NX 10 Basic Curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried going to...

 

Preferences -> User Interface -> Layout

 

...and selecting the 'Reset Window Postion' button?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: NX 10 Basic Curves

Legend
Legend
Spoiler
Spoiler
 
Yes, tried that 1st.


 Yes, tried that 1st.

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX 10 Basic Curves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you missing the tracking bar from the basic curve dialog or the basic curve dialog itself?

 

If you are missing the tracking bar, open the basic curve dialog, then follow the steps given by John. If the basic curve dialog isn't open at the time you "reset the windows", the tracking bar won't come back.

Re: NX 10 Basic Curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Has it anything to do with the ROLES. I guess the basic curves will be missing in Essentials Role.

Else you can try fetching it back from customize. (Attaching an image herewith).

Hope i understood your question clearly.

Best Regards

Kapil

lBasic

Re: NX 10 Basic Curves

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @all,

 

This is a known issue. There are existing PR's for this, and the issue is solved for NX 11.0.

 

Method to "find" it back is described above here, but you might also look at this:

http://solutions.industrysoftware.automation.siemens.com/view.php?si=001-7393714

 

As soon as you go to another application, the tracking bar will disappear again, same steps to find it back again can be used.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 10 Basic Curves

Legend
Legend

I imported my customizes Role from NX9.

 

In NX9 the dialog bar shows up fine in basic curves, just not in NX10

 

I'm refering to it as dialog bar as thats what its called in the Help.

 

 

 

 

Thanks Cowski, I didn't have the Basic curve command open when resetting the window. That fixed it.

 

dialog.PNG

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX 10 Basic Curves

Creator
Creator

I just confirmed that after upgrading to NX 10.0.3.5 MP8 , once the tracking bar is Reset, it sticks. It'll be there after application change.

 

EDIT:  If the reset is done within Modeling, it'll retain the tracking bar within modeling only. You may switch appications but in Modeling the bar will be available.

 

Andy.