Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 Ordinate Dimensioning Origin

Valued Contributor
Valued Contributor

Hello,

I'm attempting to setup an origin for ordinate dimensions at an intersection of two edges/faces, but I keep getting a message stating "No intersection point found".  While in the ordinate dimensioning command, I have it set up as Single Dimension type, and have the Set Origin reference set to Intersection point.  I have the "Face Rule" set to Single Face and the "Curve Rule" set to Single Curve.  Is there a fix for what I'm doing? 

Thanks

Ordinate Origin.JPG

3 REPLIES

Re: NX 10 Ordinate Dimensioning Origin

Legend
Legend

Try this option:

 

 2016-09-19_01.gifNX10 Two Curve Intersection

One of my favorites when dimensioning...

When you press it, you are prompted to select two lines; The result is your intersection point that you're looking for.

You may have to add this option yourself in the ribbon.

 

I hope this helps a bit.

 

Greetings,

Huysmans Metalen n.v.
2x NX 11.0.2.7 Mach Designer
on Win7 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: NX 10 Ordinate Dimensioning Origin

Valued Contributor
Valued Contributor

Perfect!  Exactly what I needed!  

 

Thanks for your help.  Much appreciated.  

Re: NX 10 Ordinate Dimensioning Origin

Legend
Legend

Smiley Wink

Huysmans Metalen n.v.
2x NX 11.0.2.7 Mach Designer
on Win7 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend