03-24-2017 12:04 PM
Hello, Whenever I am trying to assembly a part into an assembly and I select a datum plane for Touch/Align, it seems that I almost always have to select Reverse Last Constraint after selecting the datum planes in the part and the assembly. It seems like the assembled part almost always goes into the assembly opposite of how I want it to be. Is there a way to change a setting or do something so that I don't have to use the Reverse Last Constraint? Thanks
Solved! Go to Solution.
03-24-2017 12:38 PM
Are you using datum plane in the assembly and the component you are adding? You stated you are using Touch/Align, what Orientation setting are you using?
03-24-2017 12:46 PM
Yes, I was using the datum plane in the assembly and the part I'm trying to assemble. As far as the Orientation, I just had it as Prefer Touch.
03-24-2017 12:53 PM
Check the datum plane orientation directions. For Touch they will point at each other, for align they will point in the same direction. Does this help?
03-24-2017 01:00 PM
If you are using "touch" or "prefer touch" and always need to reverse the constraint, use "align" instead.
The touch and align options work based on the normal direction of the objects chosen. The "touch" option will orient one of the objects so that the normal vectors point toward each other (opposite directions), the "align" option will orient the objects so that the normal vectors point in the same direction.
03-24-2017 01:03 PM
Thanks! That's exactly what I needed. Much appreciated.