Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 10 has stopped working

Experimenter
Experimenter

Not sure if this is the correct location for this question.  I did a search and spent a few minutes looking around and have not seen anything that helps with my issue. I upgraded to IE11 a couple of weeks ago. Now when I leave NX idle for a few hours I get this error message.  "NX 10 has stopped working"  "A problem caused the program to stop working correctly. Windows will close the program and notify you if a solution is available" "Close program"

I am not sure if it is due to the windows IE11 upgrade or if it is an NX 10 to IE11 issue.  Any help will be appreciated.

See attached file for a screenshot of the error message.

 

thks,

2 REPLIES

Re: NX 10 has stopped working

Genius
Genius

Call or message GTAC, include your log files Help--> Create Support Logs for IR/PR

Re: NX 10 has stopped working

Creator
Creator

Hello,

 

did you get a solution for your problem with "NX has stopped working".
We do have the same problem when starting with Windows 10 - no similar problems with Windows 7 !

 

Regards

Wolfgang