Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.0 - Full Product Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Dear Siemens PLM NX Customer,

 

We are pleased to inform you that NX 11.0.0 is now available for download from the Siemens PLM download server.  NX 11.0.0 is available for the following platforms; Windows 64-Bit, Linux 64-Bit, and Mac OS 64-Bit.  Please refer to the Release Notes for specific Operating System requirements.

 

Please use the following steps to download the NX 11.0.0 Full Product Release.  Note: A valid WebKey account is required. 

 

In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/            

 

  • Select the "NX" product on the left hand side
  • Expand “Full products
  • Expand the appropriate platform; Linux (64-bit), MacOS or Windows(64-bit) to see a list of products and a link to download the Documentation.

 

To download the NX 11.0.0 product:

  • Right click on the nx-11.0.0 product link
  • Select "Save Target As" or "Save Link As" to save the file to your local destination.
  • Refer to the README for installation instructions

 

To download the NX 11.0.0 documentation:

  • Expand the "Documentation" link
  • Right click on the docs_help-11.0.0 documentation link
  • Select "Save Target As" or "Save Link As" to save the file to your local destination.
  • Refer to the README for installation instructions

 

Full details on NX 11.0.0 are available in the "What's New" help topic or in the "NX 11.0.0 Release Notes".  If you encounter any problems installing NX 11.0.0, please contact your local Siemens PLM Software support office.

 

Sincerely,

Ben Broad

Siemens PLM Software

7 REPLIES 7

Re: NX 11.0.0 - Full Product Release Announcement

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks Ben!

Been frothing at the mouth for months

Re: NX 11.0.0 - Full Product Release Announcement

Honored Contributor
Honored Contributor

Why go to 11?

 

Nigel Tufnel: The numbers all go to eleven. Look, right across the board, eleven, eleven, eleven and...

Marty DiBergi: Oh, I see. And most amps go up to ten?

Nigel Tufnel: Exactly.

Marty DiBergi: Does that mean it's louder? Is it any louder?

Nigel Tufnel: Well, it's one louder, isn't it? It's not ten. You see, most blokes, you know, will be playing at ten. You're on ten here, all the way up, all the way up, all the way up, you're on ten on your guitar. Where can you go from there? Where?

Marty DiBergi: I don't know.

Nigel Tufnel: Nowhere. Exactly. What we do is, if we need that extra push over the cliff, you know what we do?

Marty DiBergi: Put it up to eleven.

Nigel Tufnel: Eleven. Exactly. One louder.

Marty DiBergi: Why don't you just make ten louder and make ten be the top number and make that a little louder?

Nigel Tufnel: [pause] These go to eleven.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: NX 11.0.0 - Full Product Release Announcement

Builder
Builder
Thanks Ben.

Would you have any idea when the media will be mailed out?

For the past several versions, I have been unable to download anything from the GTAC website and I have triad all of GTAC's suggestions (different browsers, with download accelerators, without accelerators, etc.).

Thanks!

Re: NX 11.0.0 - Full Product Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
@Vikingbro - I sent you a PM.

Re: NX 11.0.0 - Full Product Release Announcement

Pioneer
Pioneer

Mr. Ben

Thanks for Announcement

 

Sudikin

NX10|TEAMCENTER10.1|

Re: NX 11.0.0 - Full Product Release Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Worked with @Vikingbro on his download issue. We were able to solve this.

 

Should you have the same problem with downloading, have a look at the following movie for an option that might help you.

 

http://www.screencast.com/t/dv1MSoXnY4gV

 

Thanks @Vikingbro for your time!

 

Kind regards

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software
Highlighted

Re: NX 11.0.0 - Full Product Release Announcement

Builder
Builder

Thank you for your assistance!