Cancel
Showing results for 
Search instead for 
Did you mean: 

NX_11.0.1_Error_In_My_System

Builder
Builder

Hello friends,

 

i updated nx to latest version 11.0.1

 

now when i open my assmebly , i got this horrible error

 

 

have anybody idea for this, if got than please help

 

 Error NX when open assembly.JPG

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer
3 REPLIES 3

Re: NX_11.0.1_Error_In_My_System

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Thomas_Roman,

 

Did you upgrade from NX 11.0.0?

And do you have this issue for more Parts/assemblies, or just this one?

 

Just to check, are you sure the update was correct? NX was not running during the update?

 

Kind regards,

 

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX_11.0.1_Error_In_My_System

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Thomas_Roman,

 

Please consider reporting this issue to GTAC, we have a couple of similar issues already being investigated so it would be good to know if yours is a new one, or a duplicate.  If your issue is closed against an existing PR you will be notified when it is fixed. Based on the reported cases, these issues do not occur in NX11.0.0 mp4.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX_11.0.1_Error_In_My_System

Builder
Builder
Understood Guys


thanks for the help, i will consider this problem to GTAC, thanks for the help, i appreciate this....

thanks again




Warm Regards
Thomas Roman
Machine Designer