Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.1 MP1 Error

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

After the NX 11.0.1 MP1 was installed, this error occurred.

 

The image is attached.

 

 

Regards,

 

Richard

4 REPLIES 4

Re: NX 11.0.1 MP1 Error

Are you sure you installed the MP in the location of NX 11.0.1?

Are you sure the MP script completed without any "file not copied" messages?

 

Mark Rief
Retired Siemens

Re: NX 11.0.1 MP1 Error

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Did you install NX11.0.1 first?

Do you use any custom programs?

You might want to give the GTAC Systems group a call.

 

Regards, Ben

Re: NX 11.0.1 MP1 Error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Richard_audie

 

2 things to check:

1) Make sure NX is not running (Check you Task manager if ugraf.exe is still running, if so, close it)

2) When you run the update, right click the file, and select, Run as Adminstrator. Even though you might be a local admin, this does give you some extra rights, so the update is successfull.

 

And like said before, if the updates ends, check if all files are copied. There should be no error message.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 11.0.1 MP1 Error

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you..

 

 

Regards..

 

 

Richard