Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Dear Siemens PLM NX Customer,

We are pleased to inform you that NX 11.0.1 is now available on Siemens PLM download server.

NX 11.0.1 is an accumulation of fixes and small enhancements built for installation on top of Windows 64-Bit, Linux 64-Bit, and Mac OS 64-Bit images for NX 11.0.0.  Please note that this Maintenance Release will only be shipped (on DVD) by request.

 

To find the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window (Note: A valid WebKey account is required):

 

      https://download.industrysoftware.automation.siemens.com/download.php

 

From the download page, enter “11.0.1" (including the quotes) in the Search field and then filter by "Product: NX" and "Platform: maintenance-release", to return a list of links to download the files appropriate for this release.

 

NX11.0.1 also includes updates for the Release Notes, What’s New and NX Help documentation.  The update is separate from the Maintenance Release package, or you can access the documentation from the Siemens PLM Doc Center website: https://www.plm.automation.siemens.com/en_us/docs/

Please refer to the README file for Maintenance Release installation instructions.

Sincerely,

Ben Broad

Siemens PLM Software

2 REPLIES 2

Re: NX 11.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

NX 11.0.1 offers over 100 user driven enhancement requests

 

Click on the links below to watch movies showing the new functionality in action:

 

  • Isolate in New Window - Allowing you to display selected components in a separate graphics window without affecting the rest of the assembly's display in the original graphics window (documentation).
  • Line Normal Enhancement - The Normal option of the Line command has been enhanced to allow selection of multiple End objects. This ensures the line updates correctly if the Start object is changed or moved (documentation).
  • Offset Curve in Face Enhancement - The Offset Curve in Face command is enhanced so you can offset a curve through a point that lies on the selected face. You may specify either the Chordal or Geodesic Offset Method (documentation).

 

Click below to read community Knowledge Base articles related to NX11.0.1 enhancements:

 

 

Regards, Ben

Re: NX 11.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor