Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.2.7 cannot open part

Creator
Creator

After a routine saving of the part file, it didn't want to open the following day.  When attempting to open, I get this error window that says, "...could not be loaded...corrupt data found when loading an OM file".

 

Here are the computer specs:

NX 11.0.2.7

Win 7 Enterprise, SP 1

Intel Core i7-6820HQ 2.7 GHz

16 GB 2133 MHz RAM

 

Thanks!

3 REPLIES 3

Re: NX 11.0.2.7 cannot open part

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @icecold1980 ,

 

Please, first confirm in what NX version the part file is saved. For that follow below steps:

 

  • Start -> Siemens XX -> NX Tools -> Command Prompt
  • Enter ug_inspect <followed by the path to your part file>

If the part is saved in the current or older version, it should open. If it does not, please contact GTAC team for further investigation mentioning the last steps performed on the part.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!
Highlighted

Re: NX 11.0.2.7 cannot open part

Creator
Creator

Samadhan,

 

Yes, output of that command confirms the file was saved in the current version.  How do I contact the GTAC team?  What does that stand for?

 

Thanks for reaching out,

 

Christian

Re: NX 11.0.2.7 cannot open part

Siemens Phenom Siemens Phenom
Siemens Phenom

Christian,

 

GTAC stands for Global Technical Access Center.

 

Please visit this site for support: Contact GTAC

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!