Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 11.0.2 - Maintenance Pack 0 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Dear Siemens PLM Customer,

Maintenance Pack 0 for NX 11.0.2 is now available on the Siemens PLM Download Server.

NX 11.0.2 MP0 fixes the issue where Weld Assistant was missing from Maintenance Release NX 11.0.2 (per PR 8920600).  This maintenance pack should be installed on top of Windows 64-Bit and Linux 64-Bit images of NX11.0.2.

To select the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Download page, enter “11.0.2.mp00” (including the quotes) in the Search box to see a list of links for the release letter and available release packages.

Alternatively, the release packages can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: Product updates > Maintenance-packs > Nx11 > [platform].

Sincerely,

Ben Broad

Siemens PLM Software

1 REPLY

Re: NX 11.0.2 - Maintenance Pack 0 Announcement

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Great response time on this - I look forward to getting more customers on to 11.0.2.