Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.2 - Maintenance Pack 3 Announcement

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Dear Siemens PLM Customer,

NX 11.0.2 MP03 is an accumulation of fixes built for installation on top of Windows 64-Bit and Linux 64-Bit images of NX 11.0.2.

To select the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Download page, enter “11.0.2.mp03” (including the quotes) in the Search box to see a list of links for the release letter and available release packages.

Alternatively, the release packages can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: Product updates > Maintenance-packs > Nx11 > [platform].

Sincerely,

Ben Broad

Siemens PLM Software

3 REPLIES 3

Re: NX 11.0.2 - Maintenance Pack 3 Announcement

Phenom
Phenom

Hi,

can someone verify if after the installation, conversion tools like step214 was removed from NX application in the start windows application ?

Menu Start.png

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: NX 11.0.2 - Maintenance Pack 3 Announcement

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @cubalibre00,

 

They're still there for me after NX11.0.2 mp3 update:

Screenshot - 10_27_2017 , 7_38_14 AM.png

 

Regards, Ben

Re: NX 11.0.2 - Maintenance Pack 3 Announcement

Phenom
Phenom

Thank you @BenBroad.

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM