Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.0.27 SAVE AS FUNCTIONS

Creator
Creator

We have upgrade from NX9 to NX11 along with many other changes, one we are concerned about is the differences in the "SAVE AS" functions.

seems there are 3 types of SAVE AS functions.

 

1. SAVE AS

2. SAVE AS NON-MASTER  PART

and 

3. SAVE AS NEW ITEM TYPE

 

 

what are the meanings of each and the impact in TEAMCENTER?

4 REPLIES 4

Re: NX 11.0.27 SAVE AS FUNCTIONS

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Treebeard67,

 

Save As with a UGMASTER as the work part: Saves the UGMASTER to a New ItemID or a New Item Revision.

Save As Non-Master with UGPART as the work part: Save a UGPART (specification or manifestation - i.e., the drawing) as a new UGPART under the same Item Revision, or under a different UGMASTER (relationship to the original UGMASTER is kept).

Save As Non-Master with UGMASTER as the work part: Save the UGMASTER as an Alternate Representation.

Save As New Item Type: OOTB, Teamcenter uses "Item" as the default item type for NX datasets.  If you wish to save your NX datasets under a different item type (e.g., Standard Part) you can use this option.

 

Hope that helps.

Regards, Ben

Re: NX 11.0.27 SAVE AS FUNCTIONS

Creator
Creator
Yes, thank you.

I am still concerned about the SAVE AS NON-MASTER part, because we have made SAVE AS TYPE changes using this function prior to the NX11.0.2.7 patch. The SAVE AS ITEM TYPE Function was not available in NX11.0.0.0

Re: NX 11.0.27 SAVE AS FUNCTIONS

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
The SAVE AS ITEM TYPE Function was not available in NX11.0.0.0

The Save As New Item Type functionality has been available for a while now, and was available in NX9 - it just had to be enabled via the Customer Defaults: Allow Save As Different Item Type".  You'll also find "Allow Save As Non-Master to a Different Item" in the Customer Defaults.

 

Regards, Ben

Re: NX 11.0.27 SAVE AS FUNCTIONS

Siemens Phenom Siemens Phenom
Siemens Phenom

In addition, once you get to NX 11.0.1 with Teamcenter the entire saving process is being streamlined to make the saving of assemblies easier.

 

See the details here.

 

NX 11.0.1 / Teamcenter Save Dialogs

 

Scott