Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Experimenter
Experimenter

Hi,

 

I would like to ask you, if somebody know (I hope yes) how to make dimension "min distance" between e.b. two radiuses or two splines, example is attached. 

Thank you in advance for any tip Smiley Happy min.distance.JPG

5 REPLIES 5

Re: NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

One option: switch to modeling and create an associative "measure distance" feature with the "create output geometry" option toggled on; use the line or points to create your dimension in drafting then hide the measurement objects.

Re: NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Gears Phenom Gears Phenom
Gears Phenom

@OJe,

 

I believe if you are using Rapid Dimension, you can change the Measurement Method pulldown to Point to Point and make sure your Snap Point setting has Tangent Point enabled.  This will work for arcs and most splines.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6

Re: NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Experimenter
Experimenter
The solution with "rapid dimension" unfortunately does not work, one point I can select with "tangent selection" but second point it is not possible select in this way. This way I can make dimension, but only by coincidence I can determine the minimum distance, it is not exact place. I tried to do new sketch where I draw a line with minimal distance, then made the dimension and at the and hid the auxiliary line. But I am not sure, that this is the right way, it looks too difficult, there should be a command for it, it is basic function available in other SW.

Re: NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What about expressions -> measure distance?

Is there a solution that leaves geometry (line or points) that you can dimension to?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 11.02 dimensioning of e.g. 2 radiuses (min. distance)

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Similar to what @cowski1 and @Ken_A suggested - create a sketch in the view on the drawing sheet.  Construct lines such that their end points are tangent to the objects being measured and parallel to each other.  Draw a line between the end points and use this to drive your dimension and then hide the sketch by clicking the checkbox under the view in the Part Navigator (part attached).  Compare your result to the Distance Measurement "Minimum Distance" command.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration