Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 11 Inter part Expressions Warning Message

Pioneer
Pioneer

Hello, 

 

When I try to open any of the Progressive Die Wizard (PDW) parts in NX11, it pops with a warning message as attached. 

1.JPGWarning Message

 

But if I open the same PDW part in NX9, I don't get the warning message. 

 

Though it preserves the expression as it is, but fails to update in the expression UI.

 

Could you please let me know the reason for this behaviour?

 

Best Regards,

Praveen 

 

 

4 REPLIES 4

Re: NX 11 Inter part Expressions Warning Message

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Praveenkumar,

 

This was a know issue, reported PR 7436467 was filed on this...

 

PR#7436467

 

Issue

===== 

Need a way to avoid the "Update event List" messages being shown every time in NX 10.0.2.6

 

Solution

========

The problem where update event list is shown when parts are missing has been fixed. A customer default has been provided in NX 11 and an environment variable has been provided in NX10.0.3 to suppress it.

 

set UGII_KF_DISABLE_MISSING_IPE_PART_WARNINGS=1

---------------------------------------------------------------------------------------------------------------------------------------------------

Since you're on NX 11.0 the variable won't work. You should use the Customer default:

File --> Ultilies --> Customer Defaults --> Gateway --> General --> Expressions --> "Show Missing Interpart Expression Part Warning"

 

Be sure to restart NX, before the settings is applied.

 

Kind regards,

 

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 11 Inter part Expressions Warning Message

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also, check your load options. It sounds like the referenced part either cannot be found with the specified options or just isn't being loaded.

Re: NX 11 Inter part Expressions Warning Message

Pioneer
Pioneer

Hello @DennisdeBrouwer

 

Thank you very much for the information, it has resolved my team's issue. 

 

Best Regards,

Praveen

Re: NX 11 Inter part Expressions Warning Message

Pioneer
Pioneer

I have checked the load options and seems to be same with both the versions of NX (NX9 & NX11)