01-27-2017 05:24 AM
Hello,
When I try to open any of the Progressive Die Wizard (PDW) parts in NX11, it pops with a warning message as attached.
Warning Message
But if I open the same PDW part in NX9, I don't get the warning message.
Though it preserves the expression as it is, but fails to update in the expression UI.
Could you please let me know the reason for this behaviour?
Best Regards,
Praveen
Solved! Go to Solution.
01-27-2017 07:42 AM - edited 01-27-2017 07:44 AM
Hello @Praveenkumar,
This was a know issue, reported PR 7436467 was filed on this...
PR#7436467
Issue
=====
Need a way to avoid the "Update event List" messages being shown every time in NX 10.0.2.6
Solution
========
The problem where update event list is shown when parts are missing has been fixed. A customer default has been provided in NX 11 and an environment variable has been provided in NX10.0.3 to suppress it.
set UGII_KF_DISABLE_MISSING_IPE_PART_WARNINGS=1
---------------------------------------------------------------------------------------------------------------------------------------------------
Since you're on NX 11.0 the variable won't work. You should use the Customer default:
File --> Ultilies --> Customer Defaults --> Gateway --> General --> Expressions --> "Show Missing Interpart Expression Part Warning"
Be sure to restart NX, before the settings is applied.
Kind regards,
01-27-2017 11:09 AM
Also, check your load options. It sounds like the referenced part either cannot be found with the specified options or just isn't being loaded.
01-31-2017 04:05 AM
Hello @DennisdeBrouwer
Thank you very much for the information, it has resolved my team's issue.
Best Regards,
Praveen
01-31-2017 07:45 AM
I have checked the load options and seems to be same with both the versions of NX (NX9 & NX11)