Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 11 Render Set options missing from view settings

Experimenter
Experimenter

Hi 

 

I want to use render sets to show a couple of hidden object through other components in a drafting view. 

 

But when I go into view settings, the render set group under Common - General is missing. 

 

I have tried checking that all groups are shown, dialogues set to more, role is set to advanced, license is mach 3 and also that visible lines are set to original. These are all the suggestions I have found. 

 

Can anyone think of the reason why render sets might be missing? Image Attached 

 

Cheers Coxy 

3 REPLIES 3

Re: NX 11 Render Set options missing from view settings

Siemens Genius Siemens Genius
Siemens Genius

Hi @Coxy,

 

Are you also using Secondary geometry settings? Toggle that off and you should be able to set the render sets.

 

Regards,

Amit

Re: NX 11 Render Set options missing from view settings

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the secondary geometry setting doesn't take care of it, try clicking on the gear icon in the settings dialog title bar and turn on "show settings (more)" and select "show collapsed groups" if it is available.

Re: NX 11 Render Set options missing from view settings

Experimenter
Experimenter

Worked perfectly thank you Amit. Now time to work out how to use it.