Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 and TC 11 preview not visible ?

Genius
Genius

Hello

I have NX 11 and TC 11.

Should the preview be visible ? I just noticed it is empty.

- Other question= Is the Teamcenter Visualization-package a default tool and can be found in every TC in some form or must it be bought ? Someone asked if I have "Teamcenter Visualization". I looked my TC's "Add Applications"-list and it is not in there...So I propably don't have it ?

Untitle12d.jpg

5 REPLIES

Re: NX 11 and TC 11 preview not visible ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Does the item revision contains a JT file?


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX 11 and TC 11 preview not visible ?

Genius
Genius

I set jtfile creation Off in customer defaults at some point.

Didn't know what to do with .JT files so I turned it off because in native it created these multiple .JT files inside the folder.

Re: NX 11 and TC 11 preview not visible ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

In teamcenter also but teamcenter use the JT files for the preview of the data.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX 11 and TC 11 preview not visible ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes you do need JT files for the viewer to work. In addition the viewer does come with different levels of functionality I am pretty sure that the "base" level is included with Teamcenter. Here is how it looks when you have a JT file.

 

TCViewer.pngTeamcenter Viewer

 

Scott

Re: NX 11 and TC 11 preview not visible ?

Siemens Legend Siemens Legend
Siemens Legend
What happens if you do a multi-select in Teamcenter ? ( select all datasets under a itemrevision)
You should get to see thumbnails of selected NX parts.

regards,
Tomas