Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 clone assembly including motion files

Experimenter
Experimenter

Hi all,

 

Recently we changed from nx 10 to nx 11 with teamcenter 10. Before we used nx 10 and teamcenter 10.

We used to clone assemblies including a motion file in nx 10 with teamcenter 10. 

With cloning an assembly in nx 11 the assembly is properly cloned. Unfortunately the motion file is not cloned.

If I do a "dry run" in the clone menu it says that motion files are included but in teamcenter the file does not show. Also when changing application to motion in nx 11 the file is without simulation.

 

Does anybody know a solution for this problem?

 

Kind regards,

Arno KleinJan

1 REPLY 1

Re: NX 11 clone assembly including motion files

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Report this to Siemens GTAC (or your VAR)

This sounds like a bug

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled