Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 for Mac OS 10.12 Sierra, Mac environment,

Experimenter
Experimenter

Hi,

 

i have given the task of writing in this post to ask if someone has recently used NX for Mac OS 10.12. Since, there is not much to read in the official post of siemens, rather than version prior to 10.12. Who could share your experience working NX on Mac OS 10.12 o Macbook pro 15"? I would thank you a lot.

 

Best Regards,

 

 

 

chui01

2 REPLIES

Re: NX 11 for Mac OS 10.12 Sierra, Mac environment,

Experimenter
Experimenter

Hi,

 

We use NX 11 on mac OS 10.12 day to day and it is stable and very dependable.

We use XQuartz 2.7.9 (NOT the later versions).

 

Only "issue" with the new Macbook pro 15" is finding a dependable mac OS comapatible 3 button wireless mouse... ;-)

 

Regards,

 

Re: NX 11 for Mac OS 10.12 Sierra, Mac environment,

Experimenter
Experimenter

Hey, 

 

Could you make a installation guide using the ug_install script? I'm getting mad to install the software, we have a university licence an I have High Sierra...