Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 memory access violation

Experimenter
Experimenter

Buonasera,

 

sto utilizzando NX11, quando vado a fare un estrusione in ambiente .par mi appare il messaggio in allegato.

 

"Errore inerno: Violazione accesso memoria" ed anche "Eccezione trovata in C++ Standard vedere il registro di sistema per ulteriore dettagli"

 

Good Evening,

 

I'm using NX 11, when i'm going to do an extrusione in the .par enviroment i see the attached message.

"Internal error: memory access violation" and Exception found un C++ standard see the system log for further details.

 

 

PROBLEM 1.JPGProblema 2 NX.PNGProblema NX.PNG

 

 

 

 

4 REPLIES

Re: NX 11 memory access violation

Legend
Legend
What happens when you change the Boolean setting from Inferred to None?

If you fail to get the error after changing the Boolean setting, then I'd highly recommend contacting GTAC.
-Tim

Re: NX 11 memory access violation

Experimenter
Experimenter

Thanks for the advice, but if i change the bolean setting from inferred to none, the system returns the error: 

 

"Exception found un C++ standard see the system log for further details." 

 

To contact the GTAC supportor there is an e-mail or just by telephone?

 

- Francesco

Re: NX 11 memory access violation

Siemens Phenom Siemens Phenom
Siemens Phenom

An error message with such a basic function would imply a software install error.

 

But best advice is as the message says, send the log file to GTAC hotline.

Steve V

Re: NX 11 memory access violation

Experimenter
Experimenter

I resolved the problem. Smiley Very Happy

 

I've updting the video card drivers and now NX11 works

 

thank you all for support.

 

- Francesco