Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 11 moving Bend Annotation's Leader ?

Genius
Genius

Hello ( Sheet metal \ Flat pattern )

I updated to NX 11 and now in sheet metal drawings I can't move the Bend Annotation's Leader line anymore it seems locked.

  • In NX 9 I could move the leader(=arrow) along the bend line to a different position.
  • Now in NX 11 the arrow is anchored(=locked) to same place.

 

4242dre.jpg

2 REPLIES

Re: NX 11 moving Bend Annotation's Leader ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if i test it on NX9 NX11 and NX12 it looks to work the same.

 

the leader is always attached to the bend line.

If you have turned on the point on curve option in the top border bar then you are able the replace the arrow on the line.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX 11 moving Bend Annotation's Leader ?

Siemens Legend Siemens Legend
Siemens Legend

If you hold down the <Shift> key as you drag the annotation, it will let you slide it along the placement curve. Once you get the leader where you want it, let go of the <Shift> key and complete the place ment of the annotation.

Regards,
Abe