Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX 11 release?

Experimenter
Experimenter

Hey Paul,

 

are there any updates due to the release plan? There are some rumors that the shipment date is delayed to fall... Maybe for some people August might be in fall, but I want to make sure that our update timeline is realistic and doesn't have to be changed again.

 

BR

Fran

Re: NX 11 release?

Siemens Legend Siemens Legend
Siemens Legend

Not sure where the rumors would come from as we were pretty clear last week at Connections during Joe Bohmans session.

 

NX 11 is due to ship in August.

 

Regards

 

Paul

 

Re: NX 11 release?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

(Rumor alert)

I heard someone (not sure who, but I believe it was Siemens person) say it might be delayed to September.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 11 release?

Honored Contributor
Honored Contributor
I heard someone (not sure who, but I believe it was Siemens person) say it might be delayed to September.

Now I read it on the internet, so it has to be true Smiley Wink

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: NX 11 release?

Siemens Legend Siemens Legend
Siemens Legend

Fran

 

BTW, which version were you planning on moving to?

 

Paul

 

BTW, I don't know the background of the rumor but I checked just in case somebody knew something that Joe Bohman who runs the NX Business and myself haven't heard, and it was confirmed back to me you can expect NX 11 first week of August.

Re: NX 11 release?

Genius
Genius
Now we have a more detailed date :-)
(from August to "first week of August")

Re: NX 11 release?

Experimenter
Experimenter

Hi, I'm working on NX10 Mach1, and realy missing the draft analisys feature... 

Is it going to be part of the Mach1 in Nx11?

Re: NX 11 release?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@tamiros wrote:

Hi, I'm working on NX10 Mach1, and realy missing the draft analisys feature... 

Is it going to be part of the Mach1 in Nx11?


Have you tried using the "slope analysis" tool? You can analyze the draft on the faces of your model with it. I actually prefer it to the draft analysis tool.

Re: NX 11 release?

Experimenter
Experimenter

no. I dont know this feature. can you explain a bit how does it help?

 

Thanks!

Re: NX 11 release?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It works much like the analysis draft command. You specify the vector direction and the faces to analyze, then it color codes the faces according to the angle to the specified vector. It is included with the modeling license, you don't need any additional special license to use it.

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_nx_analysis:id722821:xid602237