Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.0 - Maintenance Pack 1 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Dear Siemens PLM Customer,

NX 12.0.0 MP01 is an accumulation of fixes built for installation on top of the Windows 64-Bit image of NX 12.0.0.

Note that this MP fixes the CAM issue (PR 9045206) discussed here.

To select the release package for your platform click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Download page, enter “12.0.0.mp01” (including the quotes) in the Search box to see a list of links for the release letter and the available release package.

Alternatively, the release package can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: Product updates > Maintenance-packs > Nx12 > Windows (64-bit).

Sincerely,

Ben Broad

Siemens PLM Software