Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.1.7 PCB Exchange Failed to Open

Pioneer
Pioneer

 

 

NX12.01 PCB Exchange Failed to Open

 

QQ截图20180418205626.png

 QQ截图20180418205558.png

 

8 REPLIES 8

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Close and re-open NX, try to open the PCB exchange application, after you get the error message, check the NX log file (menu -> help -> log file), scroll to the bottom and look for error messages. If you cannot decipher the errors and fix them, send the log file to GTAC for help.

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @FZK,

 

Are you using a different pcb exchange patch?  What is your MAYA_PCB_DIR variable set to?

I have seen the same issue and find the solution for you...

 

Dave

 

 

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Pioneer
Pioneer

 log Eile45.png

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @FZK,

 

There's a known issue with 1201 PCB Exchange.  Please got to GTAC and download the latest patch.

2018-04-18 14_28_01-Siemens PLM Download Server - Internet Explorer.jpg

 

Replace your UGPCBEXCHANGE folder with the new content and restart NX.

Please make a back of the folder first.

I have noticed an issue with running Flexible PCD after this patch and will follow up on that issue when I have more information.

 

Dave

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Siemens Phenom Siemens Phenom
Siemens Phenom

You can login with your webkey.  If you don't have access to it, then ask your admins to do it for you?

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @FZK,

 

The product downloads page lists products that you're licensed to download.

If your maintenance is up-to-date, and your license entitles you to use NX, then NX will be listed on the downloads page from which you can download the full product and any add-ons and/or patches.

 

If your webkey is not tied to your sold-to ID (a.k.a Server ID) you will not be able to access the downloads page.  If you're unable to access the downloads page for this reason please contact your system administrator (or whoever is able to access the downloads page) rather than requesting that users of this forum send you patches.  You can also contact GTAC to request that your webkey username is tied to your sold-to so that you can access the downloads page.

 

Thank you for understanding.

Regards, Ben

Re: NX 12.0.1.7 PCB Exchange Failed to Open

Pioneer
Pioneer

I use piracy