Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.1 - Maintenance Pack 1 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Dear Siemens PLM Customer,

NX 12.0.1 MP01 is an accumulation of fixes built for installation on top of the Windows 64-Bit image of NX 12.0.1.

To select the release package for your platform click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Download page, enter “12.0.1.mp01” (including the quotes) in the Search box to see a list of links for the release letter and the available release package.

Alternatively, the release package can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: Product updates > Maintenance-packs > Nx12 > Windows (64-bit).

Sincerely,

Ben Broad

Siemens PLM Software

2 REPLIES

Re: NX 12.0.1 - Maintenance Pack 1 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

NX 12.0.1 mp01 has been temporarily recalled.

 

Regards, Ben

Re: NX 12.0.1 - Maintenance Pack 1 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

NX 12.0.1 mp01 has been re-released and available for download from the FTP server.

The fixed MP corrects the issue with the new Measure command, reported here.

Regards, Ben