Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Dear Siemens PLM NX Customer,

We are pleased to inform you that NX 12.0.1 is now available on the Siemens PLM download server.

NX 12.0.1 is an accumulation of fixes and small enhancements built for installation on top of Windows 64-Bit and Linux 64-Bit images of NX 12.0.0.  Note that while Maintenance Release NX 12.0.1 will replace the previous base installation of NX 12.0.0, it is also itself a complete base installation and therefore does not require NX 12.0.0 to be previously installed.

 

Please note that this Maintenance Release will only be shipped (on DVD) by request.

 

To find the release package(s) for your platform(s) click on the following link or enter the URL in your browser address window (Note: A valid WebKey account is required):

 

      https://download.industrysoftware.automation.siemens.com/

 

From the download page, enter “nx-12.0.1" (including the quotes) in the Search box to see a list of links to the release letter and available release packages.

 

Alternatively, the release packages can be found using the file navigator by selecting ‘NX’ from the products menu on the left and then navigating through the directory structure by selecting: Product updates -> Maintenance-release -> Nx12 -> [platform].

 

NX 12.0.1 also includes updates for the Release Notes, What’s New and NX Help documentation.  This update is separate from the Maintenance Release package and can be downloaded from the same platform folders, or you can access the documentation from the Siemens PLM Doc Center website.

Please note that the download zip file has been split into 3 smaller files using WinZip, instead of one large file.  Because of this change you will need WinZip, or 7-Zip, to extract the downloaded files.  Please refer to the README file for more information and for Maintenance Release installation instructions.

Sincerely,

Ben Broad

Siemens PLM Software

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

21 REPLIES 21

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter

Hello

I have an error when i try to update my NX12 with MP02.

This dialogbox appears 2 times. After that, setup exits.

 

nx1201_setup_error.jpg

 

Has anyone else this problem?

 

Greatings Silko

 

Re: NX 12.0.1 - Maintenance Release Announcement

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Good morning,

 

same issue here. update could not be done. Also at a win 7 machine, and a new installed win 10 machine. 

 

Workaroung only first deinstall NX12, and then installing with the update because it is now a hybrid one ( works for me) but is absolutly worst case at the moment.

 

tried in 5 machines and stopped now.

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter

Good Morning Everybody,

 

same Problem here. Can't install the Update on Windows 7 and Windows 10 (1709).


Greetings

Alex

Best Regards
Alex | Consultant @ :em.AG
NX2 - NX12 + TCIN | TCE 2007 - TC11.2

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

MR update is spilt into 3 parts.

From readme notes.

 

DOWNLOADING/EXTRACTING NX 12.0.X:

  The download zip file for NX 12.0.1 has been split into 3 smaller files using
  WinZip instead of one large file.  This has been done to make downloading
  without a download manager more reliable as the download time for each portion
  is shorter.  This is done to avoid network timeout or other issues which 
  result in failed downloads.

  Because of this change, you will need to use WinZip or 7-Zip to extract the
  downloaded files.
 
  For NX 12.0.1, there are 3 parts to the .zip file.  You will need to download
  all three parts into the same location and then use WinZip or 7-Zip to
  begin the extraction on the nx-12.0.1.zip file.  Extracting all files from
  the nx-12.0.1.zip file will extract the files from all 3 parts.  You DO NOT
  need to run WinZIp or 7-Zip against the .z01 and .z02 files.  This will be
  done automatically when extracting the .zip file.

 

Re: NX 12.0.1 - Maintenance Release Announcement

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hi Ganesh,

well then something is wired. Yesterday only 2 files have been available now that makes sence.

thx will try now

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter
Hi Ganesh,
I downloaded all 3 Parts and i used 7zip and Winzip for extract.
All looks fine.

The silent installation also doesn't run with the command in the readme.
Best Regards
Alex | Consultant @ :em.AG
NX2 - NX12 + TCIN | TCE 2007 - TC11.2

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter

@GaneshKadole

I have all 3 zip files (nx-12.0.1.zip, nx-12.0.1.z01, nx-12.0.1.z02) extracted in a folder without any errors.

Foldersize is 5,09GB.

 

I try to download the files again.

 

Edit:

Download again

all sha256 checksums are okay

update problem not solved

 

 

 

Re: NX 12.0.1 - Maintenance Release Announcement

Genius
Genius

It looks as though you need to use the latest version of 7-Zip. I was getting errors with version 16.04 but could extract the files with version 18.01.

Mike

NX 12.0.0 TC11.3 VMU 11.3

Re: NX 12.0.1 - Maintenance Release Announcement

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

So,

 

i downloaded all again, extracted to same folder all, same issue still error is same like the first post screenshot.