Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter

The problem seems to be if you download only the 3rd file (ZIP) extract it via 7-zip and start the launch.exe.

There I get an error. After that I realised to download the all 3 files and unzip again.

 

On some other machines the setup works fine, but not on my client where I have startet it the first time. All the other clients has also Windows 10 build 1709 and there it works with the same source.

 

I am removing now the hole NX12 from my client, cleanup everything and then I hope the reinstallation work completely with 12.0.1

 

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter

1. Please fully uninstall NX12 whit MP´s.

2. Install just clean NX 12.0.0.

3. After instalation NX 12.0.0  (no maintrance packs) you can update to 12.0.1.

 

It works 100%. Tried on 5 PCs

 

Of course, you need to download all 3 files. Right Click on nx-12.0.1.zip - exctract whit 7zip 64bit. After extract the folder need to be 5.09GB +-.

 

 

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello All,

 

There is a known issue with installing the update over an existing NX 12.0.0 installation which was not installed in English. All non-English installs seem to trip over this. This has been reported to development.

 

The current work around, uninstall NX 12.0.0, and directly install 12.0.1 (for 12.0.1 there is no need to have NX 12.0.0 to be installed first).

 

And yes, NX 12.0.1 is supplied in 3 files, *.zip, *.z01, and *.z02. You'll need to download all 3. Put them in the same folder and just extract the zip file, it will automatically find the 01 and 02 file.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 12.0.1 - Maintenance Release Announcement

Experimenter
Experimenter
I had english whit MP´s, and the issue was there. The problems are the MP´s (maintrance packs). Whit clean 12.0.0 works.

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

For me, the update works fine with MP's installed. But we'll mention it to development as well. Thanks!.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

SFB-NX-8001641 was recently posted.  Here's the NX portion of the bulletin:

 

Non-English installers are finding an error occurs when running the NX 12.0.1 installation as an upgrade to NX 12.0.  There was a UI change made to the NX 12.0.1 installation which is causing this error as MSI is using the non-modified cached transform (MST) for languages other than English.

 

This is a workaround that doesn't require an uninstall of NX 12.0 and can be performed on the system prior to installing NX 12.0.1 as an upgrade.

 

1. In Explorer, look in C:\Windows\Installer\{3C04623B-A1D4-4390-838B-7A8B58D4221A} for a file with a .MST extension and make note of the 4 number name for the file. ex. 1036.MST for French.
(Hint: in case you don't see the "Installer" folder, typing "C:\Windows\Installer\{3C04623B-A1D4-4390-838B-7A8B58D4221A}" into the address bar of Windows Explorer will take you to the folder).

 

2. Delete the .MST file.

 

3. Copy the same numbered .mst file from the downloaded NX 12.0.1 install location (dvdrom1201_nx\nx1201) to the C:\Windows\Installer\{3C04623B-A1D4-4390-838B-7A8B58D4221A} folder.

 

Example. Copy 1036.mst to C:\Windows\Installer\{3C04623B-A1D4-4390-838B-7A8B58D4221A}

 

Make sure there is only one .mst file (and no .MST file) in the C:\Windows\Installer\{3C04623B-A1D4-4390-838B-7A8B58D4221A} and then run the NX 12.0.1 installation.

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

For those of you who ran into this issue with non_English installers, and had not tried or wanted to use the workaround. New installation files have been posted on our download. Be sure to download all 3 zip files.

 

Extract the zip file, and it will find the z01 and z02 file, and create one extracted folder. Run the installer, and also for non-English installers all will work fine now.

 

And once more... If you have not yet installed NX 12.0.0, you can directly start with installing 12.0.1 without first the need for installing the base install. This only applies to NX 12.0.1, not for any previous releases like NX 11.0.1 etc.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 12.0.1 - Maintenance Release Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

SFB-NX-8001667 was published today (that supersedes SFB-NX-8001641) announcing the availability of updated installation files that were posted last week.

 

"The installation download files for NX 12.0.1, Simcenter 12.0.1 and Mechatronics Concept Designer 12.0.1 Maintenance Releases were updated on the GTAC download server on February 21, 2018 and given a file designation of .r1 in their name."

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 12.0.1 - Maintenance Release Announcement

Legend
Legend

I too had an error trying to start it after applying the update, an English user here... though I failed to copy it and send it in.

I ended up uninstalling NX12 and just using the NX12.0.1 as a full install and everything works fine.

 

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX 12.0.1 - Maintenance Release Announcement

Legend
Legend

See attached when _I tried to install 12.0.1