Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12.0.2 - Maintenance Pack 7 Announcement

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Dear Siemens PLM Customer,

NX 12.0.2 Maintenance Pack 7 is now available on the Siemens PLM Download Server.  This maintenance pack provides fixes built for installation on top of the Windows 64-Bit image of NX 12.0.2.

Note: The download structure on the FTP server for NX has changed, so please review the steps below to locate and download this Maintenace Pack.


To select the release package for your platform click on the following link or enter the URL in your browser address window:

       https://download.industrysoftware.automation.siemens.com/download.php

Note: A valid WebKey account is required.

From the Download page, enter “12.0.2.mp07” (including the quotes) in the Search box to see a list of links for the release letter and the available release package.

Alternatively, the release package can be found using the file navigator by selecting ‘NX’ from the menu on the left and then expand the following folders: NX Support > NX Supported > NX12 > Maintenance Packs > Windows (64-bit).

Sincerely,

Ben Broad

Siemens PLM Software

2 REPLIES 2

Re: NX 12.0.2 - Maintenance Pack 7 Announcement

Builder
Builder
Where is MP6?

Re: NX 12.0.2 - Maintenance Pack 7 Announcement

Siemens Phenom Siemens Phenom
Siemens Phenom

@gajdos , as far I know, it's wasn't planned. Hence you're not seeing it on download page.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!