Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 12 List and Angle issue

Phenom
Phenom

I am trying to drive an angle expression value down an assembly. I use Interpart expressions and link up to the top level assy expression. This works all fine. But I would like to be able to control the angles that can be set. Here I thought I would use a "List" expression type. I can create the list but I am unable to get the "driver" expression which is set an angle to accept the list input. Any suggestions on what I might be doing wrong here?Capture.PNG

8 REPLIES 8

Re: NX 12 List and Angle issue

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello Ryan,

you have to add a new expression with the formula nth().

With this string you can use the expression "Driver" and the list to select the right value from the list.

But pay attention to the units.

 

Best regards,

Christian

Re: NX 12 List and Angle issue

Siemens Phenom Siemens Phenom
Siemens Phenom

Ryan the name of the list needs to match the driving expression with the _options put on the end. See the image below.

 

List.pngPick from a list

Scott

Re: NX 12 List and Angle issue

Phenom
Phenom
I don't fully understand your answer. Can you provide an example of this?

Re: NX 12 List and Angle issue

Phenom
Phenom
Well, well. That's an interesting. I'm wondering if that is documented somewhere! If not, it really should be.
Thank you!

Re: NX 12 List and Angle issue

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Here you go:

Creating a list expression

 

Regards, Ben

Re: NX 12 List and Angle issue

Phenom
Phenom
Ben,
Now that's not fair! ;-) Who actually reads directions!
Have a great weekend.

Re: NX 12 List and Angle issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There's an acronym (or more correctly, and initialism) for that...

RTFM ;-)

(read the "F adverb of your choice" manual)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 12 List and Angle issue

Phenom
Phenom
Ken-
You're spot on! I take the responsibility for not hitting the F1 key on the keyboard..but I actually have to read the manual on my Surface Book first because the function keys are shared! I guess I have to hit the "Fn" key first!