Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12 MCD can't get OPC server

Experimenter
Experimenter

i try conncect nx to KEPServerEx ,nx display  can't get OPC server,i try ,KEPServerEx  is sucess conncect kepserver ex to plcsim,but nx can not get opc server

15 REPLIES 15

Re: NX 12 MCD can't get OPC server

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
Did you tried running NX as an admin? Sometimes the communication between NX and the OPC Server is blocked by the windows firewall.

Re: NX 12 MCD can't get OPC server

Creator
Creator

I have the same problem.

 

I have a Allenbradley  Controllogix Ethernet  PLC communication with Kepserver 6 running.

I have set NX MCD as administrator.

Still i can not get the communication between Kepserver and NX MCD running.

NX MCD is not seeing any OPC DA server.

Is there a manual how i can get this communication running.

 

Re: NX 12 MCD can't get OPC server

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Which NX Version are you currently running?

Try installing OPC Core Components V3.0++, restart NX and see if the issue is solved.

 

There's been a known issue between NX and older version of OPC Core components which could lead to the problem you described here.

Re: NX 12 MCD can't get OPC server

Creator
Creator

Where can i download OPC Core Components V3.0?

I did not find it on internet. Also not at the opc foundation!

Re: NX 12 MCD can't get OPC server

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Re: NX 12 MCD can't get OPC server

Creator
Creator

Thanks al lot. 

NX MCD is seeing the all opc servers include the Kepware server.

I

Re: NX 12 MCD can't get OPC server

Creator
Creator

I did choose in the External Signal Configuration: Kepware.KepserverEX.V6

I selected under in this window all the I/O

 

I have succesfully connected the I/O  in the signal mapping window

 

In the sequence editor i have connected this symbolic to the operations

 

so far so good.

 

But when i push the play button i get a Runtime Error window.

 

Object           Severity     Display Part                     Description

Unknown      Error          Strap_storage2_stp         Cannot connect to this OPC Server

 

Why ?

 

The External Signal Configuration:  No error with the OPC server

Signal Mapping : No error with the OPC server

 

 

Re: NX 12 MCD can't get OPC server

Experimenter
Experimenter

Hello together

 

I have the same issue as "Kaak_BG". Everything connected but when i press the play button there is this Runtime Error.

 

Does anyone has a solution for this?

 

 

Re: NX 12 MCD can't get OPC server

Creator
Creator
Hello

Siemens Germany is at this moment testing my configuration.
I hope they find a solution.
17 july 2018 a new version of NX-MCD 1202 is coming available with OPC-UA support.

Met vriendelijke groet / With kind regards / Mit freundlichen Grüssen,

Bert Gerritsen
Engineering department
[cid:image001.jpg@01D1109C.29B00880]

Kaak Nederland b.v.
[cid:80D978D1-7657-4766-9ECD-9AA7C90D6C59] P.O.Box 16, 7060 AA
[cid:B82E3CF2-F4B7-4AA3-BF69-53AC17E73F9E] Varsseveldseweg 20a, 7061 GA
Terborg, The Netherlands
[cid:F144CCDF-04F8-414B-9FC6-2137FF58561E] +31 (0)315 - 339493
[cid:24F444AD-28F0-4EBB-A7EE-DA5A27C19FBA] +31 (0)6 - 12576483
[cidSmiley Very Happy715A924-BA5B-455E-AD6B-22341B1BB92D] bgerritsen@kaak.nl
www.kaak.nl