Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 12, WIndows 10, and C++ Exceptions

Legend
Legend

I just upgraded to Windows 10 and NX12 is giving me fits with C++ Exceptions dialogs (see the log below).

 

The NVidia drivers were updated to the latest WIndows 10 ones on both an NVIDIA M3000M and a Titan XP (http://www.nvidia.com/download/driverResults.aspx/86510/ )   Running on either card gives the same problem.

 

What do you all think?  Do I need to backtrack on Nvidia drivers or is it something else?

 

*** EXCEPTION: Severe error  69 in line 210 of o:\ugnx120\ip27\src\syss\no\ind\Error_Severe.cxx at Fri Mar  9 13:28:47 2018 Eastern Standard Time
+++ C++ std::exception caught: Unknown exception
[ 1] 7FFB8133CA57                                                              (libsyss) 
[ 2] 7FFB8133C73B                                                              (libsyss) 
[ 3] 7FFB8133D03C                                                              (libsyss) 
[ 4] 7FFB8133D1BC                                                              (libsyss) 
[ 5] 7FFB8288906B                                                              (libdisp) 
[ 6] 7FFBBAA7C1E0                                                              (VCRUNTIME140) 
[ 7] 7FFBBAA72D03                                                              (VCRUNTIME140) 
[ 8] 7FFBCE3E9603                                                              (ntdll) 
[ 9] 7FFB82544F3F                                                              (libdisp) 
[10] 7FFB825445A6                                                              (libdisp) 
[11] 7FFB82544CD6                                                              (libdisp) 
[12] 7FFB825F588A                                                              (libdisp) 
[13] 7FFB826AA952                                                              (libdisp) 
[14] 7FFB826AA22A                                                              (libdisp) 
[15] 7FFB826A9F0C                                                              (libdisp) 
[16] 7FFB70E241D6                                                              (liblwksint) 
[17] 7FFB70E2519A                                                              (liblwksint) 
[18] 7FFB70E260F1                                                              (liblwksint) 
[19] 7FFB818E67D3                                                              (libugui) 
[20] 7FFB818EDC87                                                              (libugui) 
[21] 7FFB818F28D0                                                              (libugui) 
[22] 7FFB818E56F2                                                              (libugui) 
[23] 7FFB818F76C5                                                              (libugui) 
[24] 7FFB818F7F6A                                                              (libugui) 
[25] 7FFB818F4FF6                                                              (libugui) 
[26] 7FFB818E2FE9                                                              (libugui) 
[27] 7FFB81B9CF45                                                              (libugui) 
[28] 7FFB81D1A6FB                                                              (libugui) 
[29] 0000010084FD                                                              (windowsui) 
[30] 00000100D35D                                                              (windowsui) 
[31] 000001009CC0                                                              (windowsui) 
[32] 7FFB8D5301BA                                                              (mfc140u) 
[33] 7FFB8D52FCCE                                                              (mfc140u) 
[34] 7FFB8D52CF6C                                                              (mfc140u) 
[35] 7FFB8D52D344                                                              (mfc140u) 
[36] 7FFB8D3BD471                                                              (mfc140u) 
[37] 7FFBCDDBBC50                                                              (USER32) 
[38] 7FFBCDDBB80B                                                              (USER32) 
[39] 7FFB8B0A911E                                                              (OPENGL32) 
[40] 7FFBCDDBBC50                                                              (USER32) 
[41] 7FFBCDDBB5CF                                                              (USER32) 
[42] 7FFB8D514442                                                              (mfc140u) 
[43] 000000FA3320                                                              (windowsui) 
[44] 000000FA3934                                                              (windowsui) 
[45] 000000FA6513                                                              (windowsui) 
[46] 7FFB818D5B30                                                              (libugui) 
[47] 7FFB81BE4BB7                                                              (libugui) 
[48] 7FFB81B2B6F1                                                              (libugui) 
[49] 7FFBB71E4AA5                                                              (libuginitint) 
[50] 00014000719F                                                              (ugraf) 
[51] 000140003975                                                              (ugraf) 
[52] 00014000B502                                                              (ugraf) 
[53] 7FFBCDD12774                                                              (KERNEL32) 
[54] 7FFBCE3B0D51                                                              (ntdll) 
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\disp\no\ind\Display_FlushApi.cxx" at line number 244
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\disp\no\ind\dssv2_view_ops.c" at line number 1242
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\disp\no\ind\dss_view_ops.c" at line number 1066
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\ugui\no\ind\git.c" at line number 9350
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\ugui\no\ind\git.c" at line number 7458
>>>> Severe error  69 caught in file "SurfaceWnd.cpp" at line number 873
&MACRO SUB_SELECT 2
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\ugui\no\ind\uigblfunc.c" at line number 440
>>>> Severe error  69 caught in file "o:\ugnx120\ip27\src\uginitint\no\ind\clink.c" at line number 693
&MACRO MESSAGE_BOX -2, Standard C++ exception caught. See system log for details
APP_EXITED_APPLICATION_ENVIRONMENT_CALLBACK_ID UG_APP_GATEWAY.
5 REPLIES 5

Re: NX 12, WIndows 10, and C++ Exceptions

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @MarkBurhop,

 

What was your rendering style set to?  It looks like its failing with the lightworks libraries.  I would try uninstalling the graphics driver completely before reinstalling the certified driver (rather than just upgrading the driver) - this seems to have correct a lot of the C++ errors that were being raised with the translators.  Allegedly, Windows 10 updates are messing with graphics driver's registry settings.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 12, WIndows 10, and C++ Exceptions

Legend
Legend

Roling back the driver worked and NX is happy again.

 

My only problem is that I have a NVidia Titan XP eGPU set up as well.  NX doesn't support it (which is fine) but when I plug it in, it updates the driver to my M3000M internal card.

 

Thoughts?

Re: NX 12, WIndows 10, and C++ Exceptions

Experimenter
Experimenter

Hello,

My name is Manuel and I am from the NVIDIA Customer Care team.  Could you please fill out the driver feedback form below so we can look into this please?

 

https://surveys.nvidia.com/index.jsp?pi=6e7ea6bb4a02641fa8f07694a40f8ac6

 

Regards,

Manuel Guzman

NVIDIA Customer Care

Re: NX 12, WIndows 10, and C++ Exceptions

Legend
Legend

Hi Manuel!

 

Thanks for reaching out. The good news is it appears to already be fixed.  I downloaded the latest version and it all works..

 

Version:391.35  WHQL
Release Date:2018.3.27
Operating System:Windows 10 64-bit
Language:English (US)
File Size:

445.39 MB

 

http://www.nvidia.com/download/driverResults.aspx/132845/en-us

Re: NX 12, WIndows 10, and C++ Exceptions

Legend
Legend

Do you have one of those forms for Quadro drivers? After the last windows 10 update, IT pushed down to me I'm having trouble with the journal I use to export Iges/Step files.

 

>>>> Severe error  69 caught in file "D:\workdir\reference\NX1102_7\src\part\no\ind\part_load_utils.c" at line number 1129
>>>> Severe error  69 caught in file "D:\workdir\Patches\nx1102_patch\src\part\no\ind\part_load.c" at line number 10007
>>>> Severe error  69 caught in file "D:\workdir\Patches\nx1102_patch\src\part\no\ind\part_load.c" at line number 12274
Adding load status for D:\TEMP\RNew34E4B42C7cil.prt - Standard C++ exception caught. See system log for details (69)

 

 

 

Do you have one of those forms for Quadro drivers? After the last windows 10 update, IT pushed down to me I'm having trouble with the journal I use to export Iges/Step files.

 

 

 

I know a few months back our sister company had a similar issue and rolling back the video driver corrected it. 

 

I've tried the version they're using and the latest and still have issues

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro