Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 1847 Topology optimization

Genius
Genius

Is topology optimization available with NX 1847? 

27 REPLIES 27

Re: NX 1847 Topology optimization

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Javiduc,

 

Yes Topology Optimization is available with NX 1847 Series.

 

Best Regards

Fred

Highlighted

Re: NX 1847 Topology optimization

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Javiduc,

 

Search it on documentation page: 

http://lmdbuild/tdoc/nx/1847/nx_help/#uid:index

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: NX 1847 Topology optimization

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Javiduc,

 

I contacted the product manager and he expects Topology Optimization for NX 1847 to be available by the end of next week.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 1847 Topology optimization

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

@BenBroad does this mean an additional download, re-download and install 1847, update license file, MP00?

Re: NX 1847 Topology optimization

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @martinm,

 


does this mean an additional download, re-download and install 1847, update license file, MP00?

Topology Optimization is an Add-On and exists as a separate installation to NX, so you'll only have to download the Topology Optimization files and follow the installation instructions so that NX can read them.  If you don't already have the increment in your license file for Topology Optimization, then yes, you will need to obtain a new license file.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 1847 Topology optimization

Honored Contributor
Honored Contributor

@BenBroad wrote:

Hi @Javiduc,

 

I contacted the product manager and he expects Topology Optimization for NX 1847 to be available by the end of next week.

 

Regards, Ben


Will that be in the "Add-Ons" section of downloads?

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: NX 1847 Topology optimization

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @DaveK,

 


Will that be in the "Add-Ons" section of downloads?

Yes.  Since it's compiled for NX 1847, when it becomes available I would expect it to be located under "NX 1847 Series":

 

Screenshot - 1_29_2019 , 11_37_07 AM.png

 

Regards, Ben

 

 

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX 1847 Topology optimization

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Javiduc 

 

@BenBroad mentioned that it will be an addon for download.

AFAIK, that is not up-to-date information. Starting with NX12.0.2, it is included in the Standard NX Installation.

However it needs to be activated using custom_dirs.dat.

It is located in the Subfolder "TOPOLOGY_OPTIMIZATION" of your NX Installation.

 

Johannes

Re: NX 1847 Topology optimization

Legend
Legend

Hi @Johannes_H,

Did you manage to make it work with NX1847 ?
I'm not able to enable topology optimization whether it is with the custom_dirs.dat or the environment variable.

best regards,

Frédéric.