Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX 5 Quick Extend feature

Creator
Creator

I have looked everywhere for the Quick Extend feature... can anyone point me in the right direction?

 

is it possible my install doesnt have this feature?

8 REPLIES 8

Re: NX 5 Quick Extend feature

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

it's only when you are in the sketcher and you have to turn on from the sketch toolbar (see image below).

 

2016-12-12_10-38-14.jpg

Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: NX 5 Quick Extend feature

Siemens Phenom Siemens Phenom
Siemens Phenom

It is still avaialable in all releases of NX. Here is where it is in Direct Sketch

 

QuickExtend.png

 

And if you use Sketch Task it is on the ribbon.

 

SketchTask.png

 

Scott

Re: NX 5 Quick Extend feature

Genius
Genius

Command Finder is your friend.

Re: NX 5 Quick Extend feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@elopategui wrote:

Command Finder is your friend.


If only it existed in NX 5...

Re: NX 5 Quick Extend feature

Siemens Phenom Siemens Phenom
Siemens Phenom

It does exist in NX 5.0. You can find it under: "Help" --> "Command finder"

 

Or use the Command finder to find it Smiley LOL

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX 5 Quick Extend feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

My apologies; I didn't remember command finder showing up until NX 6, but now I know why: the company I worked for at the time jumped from NX 2 to NX 6.  Smiley Embarassed

Re: NX 5 Quick Extend feature

Creator
Creator

Thank you for the help!

Re: NX 5 Quick Extend feature

Creator
Creator

Totally agree!