Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 8.0 installation error

Experimenter
Experimenter

Hi Everyone,

 

I have been trying to install NX8 in my new windows 10 Machine. I installed "License Server' successfully. Then I was trying to stop server for NX installation, but its giving problems. Without, stopping server, NX is installing fine. but again its not opening NX home page.

 

I am no techie, help me out guys.

7 REPLIES

Re: NX 8.0 installation error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hi,

Is there an error message?

~Sen

Re: NX 8.0 installation error

Experimenter
Experimenter

Thanks for replying so quickly. I had tried to install NX 8.0 earlier 4-5 times but no error message appeared. But this time, It's showing error message.

Re: NX 8.0 installation error

Solution Partner Legend Solution Partner Legend
Solution Partner Legend
Hello.

First Check your environmental variables of your computer.
make sure that UGII_LICENSE_SERVER has the correct settings 2800@"yourcomputername"
If your settings for this is correct.
Try to restart the license server.
Start LMTOOLS.
go to Start/stop/reread tab.
Stop the server.
Reread the license File.
Then Start the server again.

Hope I could help you!
~Sen

Re: NX 8.0 installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Jahnsen wrote:
make sure that UGII_LICENSE_SERVER has the correct settings 2800@"yourcomputername"
~Sen

That is typically 28000@computername

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX 8.0 installation error

Experimenter
Experimenter

Thanks guys for help. I tried all the methods carefully but the issue remains unresolved. I tried installing NX 7.5 on the same windows 10 machine. its installed properly but again the error message is displayed at the start on the NX 7.5 programe and it closes suddenly.

 

Message displayed is attached in the JPEG form.

Re: NX 8.0 installation error

Are you sure you have a valid license file for your site ID?

Have you looked at the syslog? It should have more details on why NX did not start. 

 

Mark Rief
Retired Siemens

Re: NX 8.0 installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also look at the license server log file.

If you see no license messages (either checkout or failure) then there is a "network" issue between the license server & the client (or the client never gets to the point of trying to talk to the license server).  If you are checking out a valid license, then you know the issue is on the client.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled