Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 8.5 - Origin tool dialog memory

Legend
Legend

Hello everyone

 

Is there a way to activate the dialog memory for the origin tool in the drafting application? I always end up using the same offset values and it's frustrating to have to input the same values all over again, and again and again...

 

origin tool.png

 

Does this behave the same way in NX 10? I yes, I will submit an ER.

 

Laurenj.

3 REPLIES 3

Re: NX 8.5 - Origin tool dialog memory

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes it does.  That is an old style dialog and until it gets 'refreshed' it's unlikely that anything will change.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: NX 8.5 - Origin tool dialog memory

Legend
Legend

Thanks John! I will fill out an ER tomorrow.

 

Laurenj.

Re: NX 8.5 - Origin tool dialog memory

Pioneer
Pioneer

IR 7515075 submitted!!

 

Since I'm on the subject, another pet-peeve (shoud I create a new thread?):

During the creation stage of let say a feature control frame, when the origin tool is used with the the offset  character method, once the aligment annotation is selected,  the origin tool is closed and the feature control frame dialog proceed to the creation of the next  frame, leaving you with no option to control the position of the previous one !!!

 

Does this behave the same way in NX 10? I yes, I will submit an another IR.

1.png

 

2.png

 

 

3.png

 

Laurenj