Cancel
Showing results for 
Search instead for 
Did you mean: 

NX 9 Fit plane to surface

Experimenter
Experimenter

Hello,

 

I'm looking for a way to fit a plane to a surface. Unfortunately, I just can find the fit surface function(Reverse Engineering Tab) for facet bodies to fit a plane. It doesn't work for surfaces, though.

Do you know a function to fit a plane to a surface or a possibility to convert a surface to a facet body?

 

Thank you very much for your help!

1 REPLY 1

Re: NX 9 Fit plane to surface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

One option would be to create a point set on the surface, then use the "fit surface" command (type: plane), using the point set as the input for the fit surface.