Cancel
Showing results for 
Search instead for 
Did you mean: 

NX_Cad_Drafting _Views_Error

Builder
Builder

Hello guys,

 

i have a problem

 

when i do drafting of model , 

 

i cant see part properly

 

the part image is attached with  drafting image.....

 

 

thanks

 

ThomasRoman

Machine Designer

Warm Regards
Thomas Roman
Machine Designer
12 REPLIES 12

Re: NX_Cad_Drafting _Views_Error

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Hard to say... maybe try the Hidden Line 'Show Edges Hidden by Edges' view settings? How does the same view look in Modeling using the Static Wireframe and Wireframe with Hidden Edges Rendering Styles? Can you upload the part?

Regards, Ben

Re: NX_Cad_Drafting _Views_Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Was this part modeled in NX or has it been imported? There are a number of strange face edges shown in the model view screenshot. I would guess the file has some geometry errors. Geometry errors can lead to drafting view errors.

 

If the part has been imported, you might try the "heal geometry" command to help clean it up.

Re: NX_Cad_Drafting _Views_Error

Builder
Builder
Already do that , but same problem i am facing

i think its graphics problem in system

because same problem in picture in model

cant see it properly

Regrards ,

Thomas
Warm Regards
Thomas Roman
Machine Designer

Re: NX_Cad_Drafting _Views_Error

Builder
Builder
i also seen that

i cant see model properly

i think there is some graphics problem


Regrards ,

Thomas
Warm Regards
Thomas Roman
Machine Designer

Re: NX_Cad_Drafting _Views_Error

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Not necessarily graphics at this point. It could be part specific. Do you have other parts that fail similarly?
Was the data imported? If so, what type of data (IGES, STEP, Parasolid)?
Does it fail examine geometry? If it does, post a screenshot of the failures.

Regards, Ben

Re: NX_Cad_Drafting _Views_Error

Builder
Builder

I sent my Examinme Geometry Screenshot

 

I think u r right 

 

& There is error in all part like this

 

What is the solution for it

 

 

Regards

Thomas

 

Warm Regards
Thomas Roman
Machine Designer

Re: NX_Cad_Drafting _Views_Error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Thomas_Roman,

 

There is nothing wrong with the parts in these examine geometry.

The only one that "Fails" are the smooth edges. This is true, because the parst do ahve some sharp edges.

This is not a (big) issue. To Explain: A "bol" will pass. a simple cube not. This options is just to check, if there are no unwanted edges when the surface should have been smooth.

 

I some asks, did the geometry check pass. most importantend things to look at would be:

- Consistancy

- Self-Intersections

- Spikes/Cuts

- Missalligned

 

Especially the the smootness and "tiny", are things you should normally not worry about, unless this is something you actually want to check/avoid.

 

Hope this helps.

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX_Cad_Drafting _Views_Error

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Do these parts also exhibit the incorrect edge display issue that you initially reported?

Regards, Ben

Re: NX_Cad_Drafting _Views_Error

Builder
Builder

Hello guys , 

                    You are Right from your side guys

                    But i cant get my solution

 

                  I tried same part in my laptop system in Drafting view Complete shown as part.

                 

                   But in office system the part not shown properly 

 

                 see the screenshot for detail, what i wanna say.

Regards,

Thomas

 

 

 

Captured_Office_System_screenshot.JPGCaptured_Office_System_screenshotCaptured_My_Laptop_system_Screenshot.JPGCaptured_My_Laptop_system_Screenshot

Warm Regards
Thomas Roman
Machine Designer