Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Converts part from Inch to Metric

Pioneer
Pioneer

When I bring a part in that was modeled in Inches UG converts it to metric.   I have to use the command prompt to convert it back.   

 

What is causing this and how do I stop it from happening?  

 

Thanks!

 

FMJ

5 REPLIES

Re: NX Converts part from Inch to Metric

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

"When I bring a part in that was modeled in Inches UG converts it to metric."

 

Where did the file originate (native NX file, parasolid, STEP file?) and what steps are you using to "bring it in" to NX (file open, file import, external translator, something else)?

Re: NX Converts part from Inch to Metric

Pioneer
Pioneer

I'm using "File Open." Part came from Solidworks.  Format was Parasolid X_T

Re: NX Converts part from Inch to Metric

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to set your default seed part in the NX customer defaults to a template with inch units because the default is metric.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: NX Converts part from Inch to Metric

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

All parasolid files are metric. There is no default seed file when opening a parasolid file. If you want the file to be inches, start a new inch file (using your template of choice) then use "File -> import -> parasolid..." to import the parasolid into your new inch part. NX will convert the metric parasolid file to inches upon import.

Re: NX Converts part from Inch to Metric

Pioneer
Pioneer

Awesome!   Thank you guys!