Showing results for 
Search instead for 
Do you mean 
Reply

NX Display.

Hello,

 

Having two NX licences I would like to know if there are any free NX Display, only for displaying 3D pieces.

Some people in the Companny need only seeing in their computer the pieces that they have been drawn without need to buy other licences.

 

Thanks

 

Jose C.

6 REPLIES

Re: NX Display.

Hello,

I was wrong with "NX Dispay" I mean a NX or PRT VIEWER. Anybody knows some good viewer?

Thanks

Jose C

Re: NX Display.

Haven't tried it, but it seems that this can do the job:
http://www.cadcam-e.com/freecadviewers-CATIA-STEP-IGES-Parasolid-NX.aspx

MSV
NX 9.0.3.4
NX 11.0.0.33

Re: NX Display.

I think Siemen's methd of doing this is to create JT files and use JT2Go.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be steemed than diseaseled


Re: NX Display.

That is what I was going to recommend as well. JT2Go viewer is free.

Re: NX Display.

creating additional files defeats the purpose of a viewer.
Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 11.0.2.7 / Autoform r7 /WorkNC 2017 r2
Testing:NX12 EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro K2200 on Win10 Pro

Re: NX Display.

Thanks. It's works. !

 

Good day

 

Jose C