Cancel
Showing results for 
Search instead for 
Did you mean: 

NX_Drafting_Expressions_Vaue_Edit

Builder
Builder

Hello Guys ,

 

Please see the link of discussion:- 

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Drafting-Feature-Edit/m-p/364715

 

as per our last discussion

 

I got it that we can't direct insert dimension via features in drafting

 

but we can change dimension via Expression in drafting module,

 

,but is there any option to add expression dimension/values in drafting view via any command!!!!!!!!!!

 

 

anybody have idea than please share it guys

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer
15 REPLIES 15

Re: NX_Drafting_Expressions_Vaue_Edit

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi Thomas, I have no idea what is the real objective behind your question but you can make EXPRESSIONS available wjhile in drafting. Attaching one image herewith. Best Regards Kapil

Re: NX_Drafting_Expressions_Vaue_Edit

Builder
Builder

hello bro

 

actually i wanna insert dimension in drafting view via expression 

 

i dont wanna insert dimension after give in modeling

 

again in drafting, how many dimension i have to insert

more n more

Warm Regards
Thomas Roman
Machine Designer

Re: NX_Drafting_Expressions_Vaue_Edit

Builder
Builder

actually i am spend more time to give dimension again in drafting

 

within after give it in modeling

 

there are solution i know PMI option

 

but in PMI i have to put one more dimension

result is same 

 

you have to put one more dimension

 

if i give dimension in modeling one time 

than why should i have give dimension 2nd time

 

i am not understood this

Warm Regards
Thomas Roman
Machine Designer

Re: NX_Drafting_Expressions_Vaue_Edit

Builder
Builder
Actually

I wanna insert Expression dimension/Values in drafting view as dimension

is there any option or customization available for this


have anybody idea for this!!!!!!!!!!!!!

Best Regards,
Thomas Roman
Warm Regards
Thomas Roman
Machine Designer

Re: NX_Drafting_Expressions_Vaue_Edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"there are solution i know PMI option

 

but in PMI i have to put one more dimension

result is same 

 

you have to put one more dimension"

 

I'm not sure what you mean by "expression dimension", is this a sketch dimension? If so, right click the sketch dimension and choose "display as PMI"; you can then inherit the PMI dimensions to your drawing. No need to re-create them.

Re: NX_Drafting_Expressions_Vaue_Edit

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

"is there any option to add expression dimension/values in drafting view"

 

 

Is this a feature expression, or manually created expression used in modeling that you want to access in drafting?

 

Based on your explanation it sounds like you just want to display the value of an expression on the drawing sheet?   If that's the case, do you want to show it as a dimension, a note, in a table or some other way?  All of these can be done.  If you can provide a little more information (screenshots?) we can try to help.

 

Ben

Re: NX_Drafting_Expressions_Value_to_dimension

Builder
Builder

hello experts,

 

i fully agreed that i can use convert as PMI of sketch dimension, that will show in drafting view as dimension

 

but what about feature dimension bro!!!!!!!!!

 

i cant insert feature dimension like extrude ,revolve , groove etc dimension in drafting view

eg. i extrude circle & substract with some limits, circle dimension will inherit if i draw circle in sketch,i will do convert as PMI & i can show it

but guys what about extrude feature ,i used that,but i cant inherit direct dimension of extrude feature

 

Like i used sketch parameters cmd as screenshot , i can inherit my sketch dimension, hole dimension,

 

but where is extrude revolve, move face feature !!!!!!!!!

 

in sort my problem is i wanna inherit / access direct dimension of features like extrude

 

see the screenshot for more details

 

001.JPG01002.JPG02003.JPG03

 

any body idea for this , please share it experts

 

 

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer

Re: NX_Drafting_Expressions_Value_to_dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If it were possible to show these "expression dimensions" on a drawing (it may be, I'm not sure), you will quickly run into problems. Let's say that you draw a circle and extrude it into a cylinder then use move face on one of the circular ends: which expression dimension would you show on the drawing? The extrusion length or the move face length? Neither represent the actual length of the cylinder...

Re: NX_Drafting_Expressions_Value_to_dimension

Builder
Builder
Hello@ cowski1

i think the last used feature should be show, either you have to suppress that,
than previous feature should show,
either you have to choose manually which feature you wanna give dimension
software is just tool bro , it will do that what we require,

but if i give dimension in feature than why cant software take that dimension, why should i give one more dimension in dimension , why i cant take dimension from direct feature like legacy sketch parameters or from expression
is i am true or wrong


Warm Regards
Thomas Roman
Machine Designer