Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Drafting Sheet Numbering - Start Number Choice

Experimenter
Experimenter

The part I'm working on has multiple drawing partfiles, due to its sheet number size (some of our drawings clock in at around 90ish sheets). I want to know if there a way of starting the sheet numbering in the second and third partfiles from (e.g.) 30 and 60, so I can use the <W@$SH_SHEET_NUMBER> attribute to control the sheet numbers within the drawing sheets rather than manually modifying it? When I've tried to change it, it lists the error of 'not being in sequence'.

 

2 REPLIES 2

Re: NX Drafting Sheet Numbering - Start Number Choice

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Pigeon ,

 

If you change Initial Sequence Number in Drafting Preferences, sheets number are accordingly changed.

 

SN.JPG

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: NX Drafting Sheet Numbering - Start Number Choice

Experimenter
Experimenter
Thanks, that has worked perfectly!