Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Drafting

Pioneer
Pioneer

In solidworks, we can easily hide tangent lines but in NX drafting I can't. Can I do?

5 REPLIES

Re: NX Drafting

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Easy option: in the drafting view preferences, turn off the "smooth edges" option. This will turn off all the tangent lines shown in the view.

 

Less easy option: using view dependent edit you can delete all or part of any drafting curve that you choose.

 

Hard option: plot the drawing and use whiteout.

 

Edited for completeness. How's that, 1u7obd?

Re: NX Drafting

Siemens Legend Siemens Legend
Siemens Legend

Cowski, you forgot the word 'easily'. :-)

Re: NX Drafting

Pioneer
Pioneer

cowski, your answer is correct and it enhances my knowledge.

But When i use smooth edges option it not works similar to solidworks.

what i mean to say is that it removes that portion that i doesn't want to remove but in solidworks it works fine.

Re: NX Drafting

Phenom
Phenom

1u7obd wrote:

Cowski, you forgot the word 'easily'. :-)


 

 

When you don’t know that there are other ways of doing things much easier, it’s may be possible to believe in NX’s user friendliness.

 

NX’s mindset must be “When MBD is implemented, those 2d drafting will be obsolete”. So implement MBD! Smiley Happy

 

For simple instance: In a NX drawing, how many clicks needed to change “show/hide hidden lines” where as in other software it’s just click of a button. Same buttons used in Modeling!

Oh yes, I forgot it’s possible in NX, we have to build a custom program for it.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: NX Drafting

Pioneer
Pioneer
Sorry, Fernando I doesn't get your point.