Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Export error about DWG image ..

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Guys

 I have question NX11 dwg export

 When the following drawing is converted, the image does not appear in the isometric view. 

Do I have to Setting ??  

 

캡처1.PNGNX캡처.PNG2D CAD

2 REPLIES 2

Re: NX Export error about DWG image ..

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @yjnoh ,

 

This behavior is also observed in NX1847. I could not find any IR/ER related to it.

You better contact GTAC.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: NX Export error about DWG image ..

Siemens Legend Siemens Legend
Siemens Legend

Hi @yjnoh ,

Try to export dwg with below setting. 

Autocad DXF/DWG export wizard > Input and Output > Export as > 3D

Hope it helps.

Thanks,

Amol