Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Freeze Persistently and Unfreeze

Experimenter
Experimenter

Could some one help in toggling these options for a part through an expression control in an assembly.

 

say for Example I have an expression

 

Wave Control = "XXXXXXXXX"

 

If i change the expression to  ----  Wave Control = "Freeze Persistently"   -- then the part would freeze in wave context

Similarly if i change to   ----- Wave Control = "Unfreeze"  --- the part should be Unfreezed in the Wave

 

Thank you.

3 REPLIES

Re: NX Freeze Persistently and Unfreeze

Siemens Phenom Siemens Phenom
Siemens Phenom
I don't believe you can toggle a frozen status using expressions. AFAIK, this can only be done using the Associativity Manager.

Regards, Ben

Re: NX Freeze Persistently and Unfreeze

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or an API program/journal

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX Freeze Persistently and Unfreeze

Experimenter
Experimenter

Thanks a lot for your help.

I was curious on whether it can be controlled through an UI.

and  thinking of option in a very simplistic manner without using a Journal.