Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Hole Table hole number with second Hole Table

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi all

If we create second Hole Table. Hole number will count from last number of first hole table.

Can we setting hole number on second Hole Table start from 1 for every table?

NX11.0.2

Thank you.5-1-2018 11-02-48 AM.jpg

1 REPLY

Re: NX Hole Table hole number with second Hole Table

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if think it's better that you don't have the same number twice on the drawing.

So you are sure which table is for which view.

 

Other wise if someone makes a mistake the can use the wrong table for the wrong view.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions