Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX MCD take over Operations from Subassembly

Valued Contributor
Valued Contributor

Hello,

i want to take over all operations from a subassembly.

For physyc object it is simply: right click on the object and "change owner component", but for operations i dont find any similar.... Smiley Sad Any Idea?

 

2 REPLIES 2

Re: NX MCD take over Operations from Subassembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @CSDI,

 

it is currently not possible to change the owner component for an operation. Not in NX 12 and also not in the NX January 2019 Release. You can request an Enhancement Request at GTAC. I may be wrong but I believe this is not a common use case and therefore will probably not be implemented.

 

Johannes

Re: NX MCD take over Operations from Subassembly

Experimenter
Experimenter

Hello, thank you for the quick reply. Smiley Happy

What a pitty, i hoped there is something Magic Button there Smiley Tongue

Yeah you are right, its not a common use case, but i think it is same for the "change the owner component" for Physik objects. (Imagine that: if i want to have the rigid bodies, sensors, collosion bodies...etc etc in the Top assembly, why not the Operations from the subassembly? They are (almost) useless without them)