Cancel
Showing results for 
Search instead for 
Did you mean: 

NX MCD

Experimenter
Experimenter

Hello everyone!

Can you help me to create a lamp in NX MCD, which is turn on after the one bottom(green) is pushed up, and work before the other bottom (red) pushed.
Снимок.PNG
I undestand, how create a changed color lamp and pushed bottoms, but my problem is in inability to create a memorization signal. Is there something simular in the NX like a Set/Reset command from step7??

 

3 REPLIES 3

Re: NX MCD

Siemens Legend Siemens Legend
Siemens Legend

Hello Mikhail,

 

an easy way to do it is with an MCD "Operation" that sets an signal to True or False, depending on which button is pressed.

I have prepared an example for you:

(view in My Videos)

 

Best Regards

Viktor

 

Re: NX MCD

Experimenter
Experimenter

Hi Vbraun

 

I have seen that you have worked in many of your posts with signals, such as the xbox controller or the push button. I was wondering if you could help me with a problem i have been facing lately. I need my mcd model to act when it receives extern signals but do not know how to do it. I would be very grateful to be helped by you.

Best regards

Cirnia

Re: NX MCD

Siemens Genius Siemens Genius
Siemens Genius
Hi Cirnia,

you can use signals as a condition of operations. So the signal then would trigger for example the first signal of a sequence of signals.

Regards

Jochen

-----------------
Siemens Industry Software GmbH; Anschrift: Franz-Geuer-Str. 10, 50823 Köln; Gesellschaft mit beschränkter Haftung; Geschäftsführer: Urban August, Daniel Trebes; Sitz der Gesellschaft: Köln; Registergericht: Amtsgericht Köln, HRB 84564
Sam Kuan