Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Monthly Update (NX 1855) is available for download

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Affected Software: NX 1847 SERIES
Scope: WINDOWS 64-BIT


Dear Siemens PLM Customer,


We are pleased to inform you that the latest product release of NX is now available for download from the Siemens PLM Download Server.

 

Download of NX on Windows 64-bit

Please use the following steps to download the NX product release and its documentation.
Note: A valid WebKey account is required.

• In your browser's address field enter the URL: https://download.industrysoftware.automation.siemens.com/
   Login using your WebKey username and password

• From the Download page, enter "SiemensNX-1855_wntx64" (including the quotes) in the Search field to return a list of links for the Release Letter and the Release Packages.

• Alternatively the NX product release can be found using file navigator by entering NX into the Product Filter feature on the left of your browser and then navigating through the NX directory structure as follows:
      o Expand the "NX" folder
      o Expand the "NX 1847 Series" folder
      o Expand the current release folder; "NX 1855"

 

 Screenshot - 3_14_2019 , 1_27_33 PM.png

 

To download the NX product:
      o Right click on the Release Package files
      o Select "Save Target As" or "Save Link As" to save the files to your local destination

 

• When an NX series is replaced by a newer version, the previous version (including its documentation) will be moved to the "NX Supported" folder within the "NX Support" folder. For example, NX 1851 can be downloaded as follows:
      o Expand the "NX Support" folder
      o Expand the "NX Supported" folder
      o Expand the "NX 1847 Series" folder
      o Expand the available release name; "NX 1851"

 

Screenshot - 3_14_2019 , 1_30_33 PM.png

 

NX 1847 follows this strategy and can be downloaded from the "NX 1847 Series" folder as shown below:

 

Screenshot - 3_14_2019 , 1_31_41 PM.png 

 

• Once NX has been installed, on-context help will point to the GTAC online documentation by default, so you only need to download the documentation if you want to install a local documentation server.

To download the NX documentation:      

      o Expand the "NX" folder
      o Expand the "NX 1847 Series" folder
      o Expand the "Documentation" folder
      o Right click on the product documentation link
      o Select "Save Target As" or "Save Link As" to save the file to your local destination.
      In all cases, please refer to the supplied README file for installation instructions.


If you encounter any problems during this installation, please contact your local Siemens PLM Software support office.

For current information about NX including News, Events, Case Studies, Software Updates and User Group activities please visit our website by selecting the following links:

• NX:  http://www.plm.automation.siemens.com/en_us/products/nx/
• GTAC:  http://support.industrysoftware.automation.siemens.com/gtac.shtml


Sincerely,

Ben Broad
Siemens Product Lifecycle Management Software Inc.
Digital Factory Division

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

68 REPLIES 68

Re: NX Monthly Update (NX 1855) is available for download

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

My NX1851 keeps telling me that software is up to date. So much for the automatic update?

 

2019-03-15 (4).png

Re: NX Monthly Update (NX 1855) is available for download

Phenom
Phenom

Hi,

my NX 1851 doesn't find any update. What I've to check with our ITC ?

Thank you...

Using NX1867
RuleDesigner PDM

Highlighted

Re: NX Monthly Update (NX 1855) is available for download

Siemens Phenom Siemens Phenom
Siemens Phenom

@Scaffold wrote:

My NX1851 keeps telling me that software is up to date. So much for the automatic update?


Same thing here.

Re: NX Monthly Update (NX 1855) is available for download

Honored Contributor
Honored Contributor

I jsut did a new install of 1847, and I get the red light download indicator, but when I select to download and log in, I get a "Failed to download update" message.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: NX Monthly Update (NX 1855) is available for download

Valued Contributor
Valued Contributor

Hi,

 

I have the same situation, the button remain green

 

Software is up to date.jpg

 

Regards

 

Didier

 

 

Re: NX Monthly Update (NX 1855) is available for download

Phenom
Phenom

Hi,

GTAC had responded :

The NX automatic update for NX 1855 has not yet been posted.

It is not delivered via the GTAC download server, but via a third party server.

Thank you...

Using NX1867
RuleDesigner PDM

Re: NX Monthly Update (NX 1855) is available for download

Valued Contributor
Valued Contributor

Hi Cubalibre,

 

I don't understand your answer because on my screenshot, you can see the GTAC server.

 

And see the answer on the other post

 

https://community.plm.automation.siemens.com/t5/NX-Design-Blog/NX-Continuous-Release-F-A-Q/bc-p/5777...

 

We need to wait at least one week

 

Regards

 

Didier

Re: NX Monthly Update (NX 1855) is available for download

Phenom
Phenom

Hi @Didier_PSI-CAD ,

NX1851 uses the automatic update service to check if there is an update, but as I wrote, this process is NOT connected to the GTAC download server, but via a third party server, where we had discovered that could have a week of dalay.

Thank you...

Using NX1867
RuleDesigner PDM

Re: NX Monthly Update (NX 1855) is available for download

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Many software vendors that offer automatic updates are delaying the official public release for about a week.

This is done to prevent the regular user from installing an update that might have serious issues.

During the one week delay the heavy users are usually installing updates manually and testing them heavily, so serious issues would be reported early and the public release will be delayed until the issues are resolved.

You may remember that some NX releases had a MP0 released in the past or the download had been revoked to resolve serious issues.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide